Recommended computer platform 1 |
Intel i7 processor latest version with at least 6 cores or better 2 x 500 GB hard disk (RAID 1)
2 with 40 GB free space after installation of all prerequisite software and before installation of ADS-Lite software. Configure RAID 1 (mirroring) with disk write-caching turned on.
Note: Prerequisite software includes the supported operating system, database software, .NET Framework, and any other software or service packs required for your ADS configuration.
Graphics adapter (1 GB RAM, ATI® Technologies or NVIDIA® Corporation, 64-bit compatible [for 64-bit operating systems], Small Form Factor [SFF] if required) |
|
Required minimum memory 3 |
8 GB minimum, 16 GB recommended The VM host must have at least 8 GB of allocated RAM at all times. When you configure the VM, do not select the enable dynamic memory option. |
|
Supported operating systems and database software 4 |
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). Windows® 10 Enterprise LTSC (21H2) (64-bit)Database software:
|
|
Supported operating systems for Metasys client devices |
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). Apple® macOS® 10.15 Catalina Apple® macOS® 10.14 Mojave Notes:
|
|
Supported web browser software for Metasys Site Management Portal client |
Windows® Internet Explorer® 11.0.9600.18816 Update version 11.0.47 or later Note: To ensure that websites appear and function
correctly, select the Use
Microsoft compatibility lists option, found
under .
Apple® Safari® 13.1 or later Note:
Other browsers, such as Mozilla® Firefox®, may also be used but are not fully supported. You use the web browser to download the Launcher application. After you install the Launcher application, you use the Launcher, not the web browser, to log in to the Site Management Portal (SMP) user interface. |
|
Supported web browser software for Metasys UI clients |
Windows® Internet Explorer® 11.0.9600.18816 Update version 11.0.47 or later
Notes:
Microsoft® Edge® version 91 or later
Google®
Chrome™ version 91 or later
Note: Metasys UI does not support incognito mode. To exit incognito mode, click or tap the X icon of the browser window or tab and then open a new browser window or tab. For more information on incognito mode in Google Chrome, click here.
Apple®
Safari®
13.1 or later
Note: Metasys UI does not support private
browsing. To exit private browsing, click or tap Private in the browser
window.
|
|
Supported virtual environments |
Microsoft Hyper-V™ VMware® |
|
Supported user interfaces |
Site Management Portal (SMP) Metasys UI Note:
SMP requires a license at Release 12.0. The
license is available only to existing Metasys
customers.
|
|
Additional software included with the ADS Lite software download |
Microsoft .NET Framework 4.7.2 Microsoft .Net Core 3.1.21 Launcher Software |
|
Optional hardware |
Any network or local printer supported by the qualified Windows operating system |
|
Optional software |
Graphic Generation Tool CCT Software SCT Software Metasys Database Manager Metasys Export Utility |
1 Our computer platform and memory
recommendations are not meant to imply that older or slower
machines are not usable. Refer to the
Network and IT Guidance Technical Bulletin (LIT-12011279)
1 for
more information regarding computer/server
recommendations.
2 For best performance, use Serial Attached SCSI (SAS) hard drives, not Small Computer System Interface (SCSI) hard drives.
3 It is recommended to use RAM that the
computer supports.
4 Refer to the
Network and IT Guidance Technical Bulletin (LIT-12011279)
for specific Microsoft Windows
operating system settings that may be required for your
Metasys system configuration.