The network engines offer seamless integration of Modbus, M-Bus, KNX, or other third-party network to the Metasys system. The following figure shows the SNEs and SNC integrating third-party devices. A KNX IP Gateway is also shown.
Figure 1. Third-party network integration