The Simplex Fire system includes a BACnet/IP integration, which
facilitates the integration with Metasys. The Metasys system serves as a secondary fire
monitoring system that can alert more people and automate building conditions when
triggered by a fire event. The Metasys toolset is enhanced to simplify the workflow for
integrating a Simplex Fire system:
-
The process of creating the Metasys Network, Equipment and Space integrations for SIMPLEX Fire Panels is automated through an updated Mass Change Tool utility in SCT.
-
There is a better representation of mapped fire system data in Metasys.
- The Metasys UI provides a detailed view of the fire system components, and the exact location of the fire on the building and floor plan maps.