CG series and CV series Equipment Controllers - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active
At Releases 10.0, 11.0, and 12.0, we introduced the first members of a new, modernized equipment controller family that succeeds our FEC/FAC/VMA series equipment controller family. This modernized family shares similar design details, including the following:
  • Modernized packaging and styling
  • Removable screw terminal blocks
  • Decimal MS/TP address set with three rotary switches
  • More memory and faster processor
  • Background file transfer
  • Improved SA Bus commissioning
  • Models with BACnet MS/TP and N2 networking with auto-detect (CGM and CVM models)
  • Models with BACnet/IP and BACnet/SC networking (CGE and CVE models)
    Note: The CGE and CVE models can act as BACnet/SC nodes.
  • Models with an onboard display and keypad
  • Device Security (CGE and CVE models)
  • FIPS 140-2 Level 1 Compliance (CGE and CVE models)
  • Wireless ZFR and ZFR Pro support

Figure 1. CG series and CV series equipment controllers and XPM expansion modules