| Description | Supported | Comments |
|---|---|---|
| Max. number of concurrently active archives | 10 | |
| Max. number of simultaneous browser tabs or connections |
|
If additional browser tabs or connections are accessed when SCT is installed on Desktop OS, SCT does not function as expected. |
| Max. size of an active database or project in SCT | 10 GB | Using supported Microsoft SQL Server Express software. |
| No limit | Using supported Microsoft SQL Server Standard or Datacenter Software |