Smoke Control application configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

The following figure shows a configuration that complies with the UL 864 10th Edition UUKL/ORD-C100-13 UUKLC Standard for Smoke Control System listing, incorporating smoke control and non-smoke control systems. This configuration is only an example; the number and arrangement of components in your system may differ. Ensure that your system complies with all device and communication requirements and restrictions.

Figure 1. Metasys System UL 864 10th Edition UUKL/ORD-C100-13 UUKLC Standard for Smoke Control