System Configuration Tool (SCT) - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

The System Configuration Tool (SCT) supports the engineering, installation, and commissioning of your building automation system. The SCT application enables fast offline generation and Metasys UI configuration of the complete site, including point naming; integration of N1, N2, BACnet®, and LonWorks® networks; integration of Modbus, M-Bus, and KNX third-party protocols; integration of local and remote MS/TP devices; definition of tailored summaries and user views; the creation of custom control logic using a graphical user interface; and integration of building systems such as C•CURE-victor, Simplex® fire, Zettler® fire, connected lighting systems from preferred vendors, and OPC UA. SCT offers productivity features that includes the migration of supervisory devices and the mass creation of equipment, spaces, and serving relationships.

You can use SCT or System Configuration Tool Pro (SCT Pro) to manage a mixed release site of devices at Release 5.2 and later that include the SNE, SNC, Network Automation Engine (NAE), Network Control Engine (NCE), Network Integration Engine (NIE), Application and Data Server/Extended Application and Data Server (ADS/ADX), Open Application Servers (OAS), and the Metasys UI. To keep the archive database current, you can schedule regular uploads from the devices on the site.

SCT has a one-click installation. The SCT installer installs the required software prerequisites, such as Internet Information Services (IIS) and Microsoft® .NET Framework 4.7.2. If no SQL Server® is present, the SCT installer installs SQL Server 2014 Express software.

The SCT installation includes additional applications. You can use the JCT software to configure Metasys UI graphics and the display of data without a live connection to devices. You can use the Software Manager to manage licenses for Johnson Controls software and features. For example, you can apply or remove licenses for the SCT software and field controller packages.

IT Security Commitment

Metasys uses secure HTTP with Transport Layer Security (TLS) 1.3 between the SCT computer, all Metasys servers, and network engines that are upgraded to Metasys Release 9.0 and later. The encrypted HTTPS communications apply to the Metasys servers, Metasys UI, network engines, and SCT. This ensures that unauthorized users and computer hackers cannot view the contents of communications sent between Metasys equipment. By default, self-signed certificates are installed on supported products, with the option of configuring trusted certificates configured by an internal IT department or a Certificate Authority. To indicate the active security level (trusted, self-signed, or untrusted), three small security shield icons appear on the SCT login screens and on the SCT UI screens.

Johnson Controls continues to enhance the security of Metasys with the addition of signed resource files, and the pairing of supervisory devices with the site director to ensure encrypted communication.

The following table outlines the recent history of SCT, Metasys Server, and NAE Update Tool releases:

Table 1. SCT, Metasys Server, and NAE Update Tool releases

Release Date

SCT

NAE Update Tool

Metasys Server

October 2015

Release 7.0

Release 7.0

Release 7.0

September 2016

Release 11.0

Release 11.0

Release 8.0

February 2017

Release 11.1

Release 11.1

Release 8.1

August 2017

Release 12.0

Release 12.0

Release 9.0

December 2018

Release 13.0

Release 13.0

Release 10.0

October 2019

Release 13.2

Release 13.2

Release 10.1

October 2020

Release 14.0 1

The NAE Update Tool continues to be a component of the SCT install. However, we encourage you to work with SCT Pro instead of the NAE Update Tool.

Release 11.0

November 2020

Release 14.1

Release 11.0

May 2021

Release 13.3 and 14.2

Release 11.0

May 2022

Release 15.0

Release 12.0

For a list of updated features and benefits available at the latest SCT Release, refer to the System Configuration Tool Catalog Page (LIT-1900198) .

1 SCT 14.0 was discontinued when SCT 14.1 was released.