The following table describes limitations of the Metasys system network engines.
|
Maximum allowed |
NCE25 |
NAE35 |
NAE45 |
NAE45-Lite |
NAE55 |
NAE85 |
OAS |
|---|---|---|---|---|---|---|---|
| Local Field Buses (FBs) | 1 | 1 | 1 | 1 | 2 | 0 | 0 |
| Remote Field Buses (RFBs) | 0 | 3 | 4 | 0 | 6 or 7 | 16 | 16 |
| Total Field Buses (Local and Remote Field Buses) | 1 (1 FB + 0 RFB) | 4 (1 FB + 3 RFB) | 5 (1 FB + 4 RFB) | 1 (1 FB + 0 RFB) | 8 (2 FB + 6 RFB or 1 FB + 7 RFB) | 16 RFB only | 16 RFB only |
| MS/TP devices on FC Bus
1
Note: N2 devices follow the same rules as MS/TP
devices, but performance varies based on controller mix
(N2Open/Sys91/VMA).
|
Per trunk device limits if all devices are Metasys family devices, such as CGMs, CVMs, FACs, FECs, VMAs, IOMs, and TEC3600s: | ||||||
| 32 | 50 | 100 | 100 | 100 | N/A | N/A | |
| Per trunk device limits if one device is a non-Metasys family device, such as a Facility Explorer device, TEC2000, or third-party device: | |||||||
| 32 | 50 | 64 | 64 | 64 | N/A | N/A | |
| Remote MS/TP devices on remote field bus 2 | N/A | 16 or 32 | 16 or 32 | N/A | 16 or 32 | 16 or 32 | 16 or 32 |
| Mapped N2 points per trunk 3 | 2,500 | 2,500 | 2,500 | N/A | 2,500 | N/A | N/A |
| LonWorks devices 4 | 32 | 64 | 127 | N/A | 255 | N/A | N/A |
|
Note: The LonWorks integration is only supported on
NAE35s, NAE45s, and NCE25s with the Metasys Release 9.0 software
or earlier. Patch updates 9.0.7 and later are not supported for
these LonWorks models; they remain at Release 9.0. However, the
LonWorks integration is supported for NAE55s at Releases 10.0,
10.1, 11.0, and 12.0.
|
|||||||
| LonWorks network variables | 1,500 | 1,500 | 1,500 | N/A | 2,000 | N/A | N/A |
| Johnson Controls BACnet/IP devices and third-party BACnet/IP devices | 50 5 , 6 , 7 | 505 , 6 , 7 | 505 , 6 , 7 | 505 , 6 , 7 | 2005 , 6 |
1,000 Note: Before 11.0, the NAE85 supported 200 devices.
|
200 |
| Objects | 2,500 | 2,500 | 2,500 | 2,500 | 5,000 | 10,000 (default) 25,000 (upgrade) | 20,000 |
| Time on battery backup | 1,024 seconds | N/A | N/A | ||||
See SNE Series Network Engines for details about SNE Series of Network Engines and see SNC Series Network Control Engines for details about SNC Series of Network Control Engines.
1 Maximum 3 bus segments per FC Bus. Maximum 50
devices per bus segment. Bus segments on an FC bus are connected
with repeaters (only). Up to two cascaded repeaters may be
applied to an FC bus (to connect three bus segments).
2 The maximum
device count is 32 if the bus contains all Johnson Controls
devices, and 16 if the bus contains one or more non-Johnson
Controls devices.
3 Performance varies based on the point mix (N2
Open/Sys91/VMA). Recommend maximum for best performance is 1,000
points.
4 Single sub-net LonWorks
network; does not support routers; supports physical
repeaters
5 Depends on the number of
objects each BACnet device supports.
6 Johnson Controls IP controllers only work with
NAEs (and site directors) at Release 9.0 or later.
7 Some sites may require manual mapping based on system
architecture. They may also require system adjustments, such as
BACnet communication adjustments, or firewall off.