VMD Generator Express (VGE Tool) - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

The VMD Generator Express (VGE) tool allows you to view, create, and modify the vendor model definition (VMD) files required by third-party integrations on the NIEx9. Both the TCP/IP and Remote Terminal Unit (RTU) formats are supported.

The VGE tool incorporates a version tracking system that stores data and comments every time you create or modify a file. The tool allows generic modeling for standard integrations, meters, chillers, and air handling units (AHUs).