Network Engine comparison - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active
Table 1. Network Engine Release support comparison
Model Release 9.0 Release 9.0.7 or later Release 10.0 Release 10.1 Release 11.0 Release 12.0

NCE25

X

X 1 Succeeded by SNC models, but NCE25 continues to ship out of factory at Release 9.0.7.

NAE35, NAE45

X

X 2 The SNE1050x succeeds the NAE35 series and the SNE1100x succeeds the NAE45 series, but NAE35 and NAE45 series continue to ship out of factory at Release 9.0.7.

NAE55

X

  X 3 X 4 X 5 X 6

NAE85

X

 

X

X X X 7

NIE29, NIE39, NIE49

X

X 8   Discontinued Discontinued Discontinued

NIE59

X

  X X X X
Important: All NIEx9 models have been discontinued from manufacture, because starting at 9.0.7 and 10.0, NAE models include the integration functionality of the NIE. Existing NIE59s can be field-upgraded to 10.0, 10.1, 11.0, and 12.0 respectively.
NIE89 X   X X X X
Important: All NIEx9 models have been discontinued from manufacture, because starting at 9.0.7 and 10.0, NAE models include the integration functionality of the NIE. Existing NIE89s can be field-upgraded to 10.0, 10.1, 11.0, and 12.0 respectively.

NIE55, NIE85

X

         
SNE       X X X
SNC       X X X
Table 2. Network Engine integrations available by Metasys Release
Integration Release 9.0 Release 9.0.7 or later Release 10.0 Release 10.1 Release 11.0 Release 12.0
BACnet/SC          

X 9

MQTT          

X 10

BACnet/IP

X

X

X

X

X

X

BACnet MS/TP

X

X

X

X

X

X

Legacy N1 LAN

X

         
Legacy N2 Bus

X

X

X

X 11

X11

LonWorks

X

 

X

X 12

X12

Modbus RTU and TCP

X

X

X

X

X

X

KNX IP

X

X

X

X

X

X

M-Bus Serial and IP

X

X

X

X

X

X

C•CURE-victor    

X

X

X

X

Simplex Fire (secondary monitoring only)    

X

X

X

X

Preferred Vendor Lighting Systems    

X

X

X

X

Zettler Fire Panel      

X

X

X

OPC Unified Architecture (OPC UA)        

X

X

WRS-RTN Wireless Supervisor

X

         
1 Only NCE25xx-0 is available to upgrade to Metasys 9.0.7 or later with Linux OS.
2 Only NAE35xx-2 and NAE45xx-2 are available to upgrade to Metasys 9.0.7 or later with Linux OS.
3 Only NAE55xx-2 and NAE55xx-3 are available to upgrade to Metasys 10.0 with Linux OS.
4 Only NAE55xx-2 and NAE55xx-3 are available to upgrade to Metasys 10.1 with Linux OS.
5 Only NAE55xx-2 and NAE55xx-3 are available to upgrade to Metasys 11.0 with Linux OS.
6 Only NAE55xx-3 is available to upgrade to Metasys 12.0 with Linux OS.
7 At 12.0, an NAE85 can act as a Site Director only. Do not upgrade any child NAE85s to 12.0.
8 Only NIE29xx-0s, NIE39xx-2, and NIE49xx-2 are available to upgrade to Metasys 9.0.7 or later with Linux OS.
9 NAE85, NAE55xx-3, SNEs, and SNCs support BACnet/SC.
10 MQTT is supported only on the SNC and SNE series engines from Release 12.0.
11 The M4-SNE110Lx-0 model does not support the N2 Bus.
12 The M4-SNE110Lx-0 model does not support LonWorks.