Wireless solutions - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

Several wireless Metasys solutions are available for integrating wireless connectivity in desired portions of a Metasys network. These solutions provide wireless communication between controllers, thermostat controllers, coordinators, routers, and room sensors.

  • ZFR181x Series Wireless Field Bus System
  • WNC1800/ZFR182x Pro Series Wireless Field Bus with Wireless TEC3000 Series Thermostats
  • WRG1830/ZFR183x Pro Series Wireless Field Bus with Wireless TEC31xx Series Thermostats
  • WRZ-7860 One-to-One Wireless Room Temperature Sensing System
  • TE-7800 Series One-to-One Wireless Room Temperature Sensing System

These wireless solutions reduce costs by minimizing wiring, provide application mobility and flexibility, and simplify the challenges of difficult or cost-prohibitive installations or renovations. The wireless solutions can coexist with each other, and with hard-wired Metasys solutions.