Field Equipment Controllers (FECs) | Advanced Application Field Equipment Controllers (FACs) | Variable Air Volume Modular Assemblies (VMAs) | |
---|---|---|---|
Typical applications |
Controlling:
|
Controlling:
|
Controlling:
|
Processor |
32-bit |
32-bit |
32-bit |
Onboard real time clock |
No |
Yes |
Yes - on IP VMA1930 model only |
Communication protocol |
|
|
|
Expandable through SA bus |
Yes |
Yes |
Yes |
Programmable control logic |
Yes |
Yes |
Yes |
Programming tool |
CCT |
CCT |
CCT |
Commissioning tool | CCT, MAP | CCT, MAP | CCT, MAP |
Note: You can upgrade existing VMA1930 units
in the field to support BACnet/SC, but this model is discontinued from
manufacturing.