Metasys Server Site Director with multiple network engines system configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

Sites that require more than four simultaneous users must add a Metasys Server. If a large number of graphics are required to navigate through a site, the addition of the Metasys Server allows access to a disk drive or network drive for graphic file storage. The Metasys Server provides permanent storage of collected trend data samples, event messages, and audit trail messages routed from the network engines.

Figure 1. Multiple network engines system configuration with Metasys Server Site Director