The ADX you select for a large site can be a 10-, 25-, 50-, or 100-user ADX. Refer to the Technical Specifications section of the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin (LIT-1201525), Extended Application and Data Server System Requirements (Unified ADX Systems, 50 or 100 Users) table for the technical specifications for a large ADX system.
Note: Metasys for Validated Environments supports 5, 10, 25, and 50 users.