BACnet/IP network system configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

BACnet/IP devices are connected directly to the IP Ethernet network. The network engine communicates with the devices using the BACnet protocol and presents the BACnet data to the system in the same way as the other data in the Metasys system. The following figure shows the SNE1050 integrated into the Metasys network. Other BACnet/IP devices are integrated in the same way.

Figure 1. BACnet/IP network integration system configuration
The NAE85 allows integration of larger BACnet integration projects.
Important: The following configuration is allowed with NAE85s at Release 11.0 or earlier only. At Release 12.0, the NAE85 can act as a Site Director only. In the following example, you could remove the ADS/ADX and use the NAE85 as Site Director to support Release 12.0.
Figure 2. NAE85 BACnet integration