Demand Limiting and Load Rolling - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

The Demand Limiting (DL) feature reduces utility bills by limiting peak energy usage. DL electively turns off (sheds) equipment, such as fans and lights, or adjusts setpoints to limit energy use during peak times.

The Load Rolling (LR) feature helps save money by reducing overall energy consumption. LR acts continuously to maintain a specified energy reduction by shedding unnecessary loads. A facility can implement either one or both of these features.