Equipment controller wireless integrations - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

The ZFR181x Series wireless system was introduced at Metasys Release 4.0.

  • The ZFR181x Series wireless system connects to the network engine through the FC Bus using BACnet MS/TP.
  • Wireless coordinators need to be at an equal or higher revision level than the controllers associated with it.
  • Within a wireless mesh, a mix of revisions of wireless pairs is allowed.
  • Each wireless controller and associated wireless router need to be at the same release. CCT automatically syncs release revisions between a controller and its associated router.
  • Release 4.0 controllers are not compatible with 4.1 or later wireless routers and need to be updated before connecting the wireless router.