Zettler Fire Panels - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

You can commission a Network Automation Engine (NAE), an SNE, or an SNC as a Vendor Integration for use with Zettler fire panels, which integrates data sourced from Zettler Fire Detection System into Metasys:

  • Enables Metasys to automate building conditions when triggered by a fire event.
  • Helps consolidate user experiences for building operators by enabling them to view fire equipment, trouble points and status from Zettler Fire Detection System within Metasys UI.
  • Enables Metasys to serve as a secondary fire notification system, alerting more occupants in the event of a fire.