LonWorks - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

The LonWorks network is a local operating network that was developed by Echelon Corporation. The network is built around the Neuron chip, a microprocessor that combines three CPUs into one chip. The LonWorks network uses the LonTalk® protocol, a software language for field device communication. This protocol uses the Open Systems Interconnect (OSI) reference model and features all seven communication layers for interoperability among control devices.