The SNE series network engines are the most recent family of network engines in the Metasys building automation system portfolio.
Figure 1. SNE series network engines
The following table outlines the SNE models in more detail.
| Features | SNE2200x | SNE1100x | SNE1050x |
SNE110Lx 1 |
|---|---|---|---|---|
| Succeeds | NAE55 Series | NAE45 Series | NAE35 Series | NAE45-Lite |
| Communication interfaces |
|
|
||
| Maximum number of child engines when acting as a Site Director | 3 | 2 | 2 | 0 |
| Maximum allowed devices across all integrations. For example, MS/TP+IP. Includes VND integrations and devices brought in through routers. | 600 | 150 | 60 | 110 |
| BACnet/IP maximum trunks | 1 | 1 | 1 | 1 |
| BACnet/IP maximum devices per trunk | 200 | 100 | 50 | 10 |
| BACnet/SC maximum trunks | 1 | 1 | 1 | 1 |
| BACnet/SC maximum devices per trunk 3 | 150 | 100 | 50 | 10 |
| BACnet MS/TP maximum trunks | 2 | 1 | 1 | 1 |
|
BACnet MS/TP maximum devices per trunk (Johnson
Controls devices only)
Note: A repeater is required if more than 50 Johnson
Controls devices are on the same
trunk.
|
100 | 100 | 50 | 100 |
|
BACnet
MS/TP maximum devices per trunk (with third party)
Note: A repeater is required if
more than 32 devices are on the same trunk and some are third
party.
|
64 | 64 | 50 | 64 |
| N2 maximum trunks | 2 | 1 | 1 | N/A |
|
Mapped
N2 devices per trunk
Note: A repeater is required if more than 50 devices are on the same
trunk.
|
100 | 100 | 50 | N/A |
| LonWorks maximum trunks | 1 | 1 | 1 | N/A |
| LonWorks maximum devices | 255 | 127 | 60 | N/A |
| Remote Field Bus maximum trunks | 6 | 3 | 3 | N/A |
| Remote Field Bus maximum Johnson Controls Devices per bus | 32 | 32 | 32 | N/A |
| Remote Field Bus maximum devices per bus (with third-party devices) | 16 | 16 | 16 | N/A |
| Maximum objects in device 4 | 5000 | 2500 | 2500 | 2500 |
| Supported type of parent server |
|
|
|
ADS-Lite-A only |
|
Supported integrations |
|
|||
| Operating System | Wind River® Linux LTS 17 (LTS=long-term support) | |||
| Microprocessor | NXP i.MX6 DualLite processor | |||
| Memory | Flash 2GB of DDR3 RAM and 16 GB of eMMC Flash | |||
| User Interface | Site Management Portal (SMP) | |||
1 These models are intended for use with the
ADS-Lite-A servers (only) in Australia, China, Hong Kong, India,
Indonesia, Japan, Korea, Malaysia, New Zealand, Philippines,
Singapore, Taiwan, Thailand, Vietnam, and select branches within
regions of Africa and the Middle East.
2 Only the supported USB integration adapters
function with the SNE. Other integration adapters that are
not supported cannot function with the SNE.
3 Multiple IP integrations can be on an
engine, including BACnet/IP and BACnet/SC, but this is limited by
the maximum devices that can be mapped to a trunk. The total number
of BACnet/IP or BACnet/SC devices that you can map is 150. You
cannot map 150 IP and 150 SC devices at the same time because they
use the same BACnet Integration object.
4 Suggested object limit for performance considerations.