Encrypted email - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

Metasys software features an email encryption capability that encrypts user names and passwords as they are entered into the SMP UI. Embedded and server machines can thereby send emails to email servers over a secure channel (secure socket layer [SSL]). The entire email payload is encrypted, and allows Metasys software to communicate to email servers that require SSL connections.

Users can configure email encryption with no authentication required, including SMTP authentication, and POP-Before-SMTP authentication.