Controller Configuration Tool (CCT) - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active
You can use the Controller Configuration Tool (CCT) to configure, simulate, commission, and transfer application files to the following:
  • CG series General Purpose Application Equipment Controllers
  • FAC series Advanced Application Field Equipment Controllers
  • FEC series Field Equipment Controllers
  • CV series VAV Box Controllers
  • VMA series VAV Box Controllers
  • VAV series VAV Box Controllers
  • XPM series I/O Expansion Modules
  • IOM series I/O Expansion Modules
  • SNC series Network Control Engines
  • NCE series Network Control Engines

CCT operates in the following three modes that provide key functionality for your system:

  • Use the Configuration mode to select mechanical and control logic options for typical air handling, terminal unit, central plant, and VAV box mechanical systems. You can customize the standard logic provided by the system selection process to meet your specialized control logic requirements.
  • Use the Simulation mode to review the application logic as if you were commissioning the system. You can make adjustments to setpoints, inputs, or sensors during a simulation session to validate the logic before assigning the configuration to a specific controller. A simulation debugging console is also available to setup break points that pause the simulation session based on criteria that you set up. While viewing a simulation session, transitions taking place in the logic are highlighted for a few seconds to help you quickly identify where the changes occur.
  • Use the Commissioning mode to connect to a device and view actual data from that device. You can use this mode to monitor your device and set offsets, COVs, and polarity in addition to other parameter and detail changes.

For VAV box applications, CCT includes an optional box flow test to automatically exercise all the VAV boxes to ensure correct mechanical installation and correct configuration of the key flow setup parameters.

The ZFR Checkout Tool (ZCT) is available to validate the wireless connectivity and health of your wireless mesh network. Refer to the ZFR Checkout Tool Help (LIT-12012292) for details.
Note: ZCT is not compatible with the WRG1830/ZFR183x Pro Series.

Controller Application Files (CAFs) can be transferred and commissioned to a device through a wide variety of connection interfaces, including NxE Passthru, MAP 4.2+ / BACnet® router, ZigBee®, and Direct Ethernet.

For information about upgrading or installing CCT, refer to the CCT Installation Instructions (LIT-12011529).

For a list of updated features and benefits available at the latest CCT Release, refer to the Controller Configuration Tool (CCT) Catalog Page (LIT-1900386).