MQ Telemetry Transport (MQTT) - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active

MQTT is an OASIS standard messaging protocol for the Internet of Things (IoT). MQTT is designed as an extremely lightweight publish/subscribe messaging transport that is ideal for connecting remote devices with a small code footprint and minimal network bandwidth.

From Release 12.0, the SNE and SNC series network engines include an MQTT driver that supports bidirectional communication between network engines and a generic MQTT broker.