The following tables describe performance guidelines and limitations of the Metasys system Site Directors.
Maximum allowed | Type of Site Director | |||||||
---|---|---|---|---|---|---|---|---|
NAE35 SNE1050x |
NAE45 SNE1100x |
NAE55 SNE2200x |
NAE85 |
NCE25 SNC replacements of NCE25 1 |
||||
Total engines | 3 | 3 | 4 | 4 | 1 2 | |||
Simultaneous SMP users | 2 | 2 | 4 | 10 | 2 | |||
Objects in device 3 | 2,500 | 2,500 | 5,000 | 25,000 | 2,500 | |||
Objects within a single folder | 300 | 300 | 700 | 700 | 300 | |||
Dynamic values per graphics | 100 | |||||||
Results displayed in a global search | 500 | |||||||
Languages | 1 | |||||||
Objects in entire system | 3 million/ 750k (for ADX Site Director Only) | |||||||
Characters in the name of an object | 400 | |||||||
Characters in the description of an object | 64 | |||||||
Nesting levels for object creation | 7 | |||||||
Extensions per object | 10 | |||||||
Sets for third-party BACnet states text | 1,000 | |||||||
Characters for a third-party BACnet states text | 60 | |||||||
Members for a multi-value third-party BACnet states text | 500 | |||||||
Non-Simultaneous SMP users | Limited only by memory capacity | |||||||
SMP user views | Limited only by memory capacity | |||||||
Simultaneous browsers per client computer | 2 (Mix of online, SCT, and Simulation) | |||||||
DLLR load extension | Limited only by memory capacity. If you plan to attach a large number of load extensions to a single DLLR object, consider the memory limitation. For load extensions attached to one DLLR object, there is a 64 KB text limit for the list of the Loads fully qualified references. Load Limit = (64 x 1024)/average number of characters per load. 1024 Bytes equals 1 KB. For example, if your DLLR object is configured with Loads that have fully qualified references that average 100 characters (including dots) in length, then you can support approximately 650 loads (64 x 1024/100) for that DLLR. If you reach the memory limit, you may need to combine loads. For example, if a site has multiple physical meters, split the meters across multiple controllers and apply appropriate DLLR loads, if possible. Otherwise, use Interlock or Multiple Command objects to reduce the number of loads added to the DLLR. | |||||||
DLLR objects | Limited only by memory capacity. |
Maximum allowed |
Type of Site Director |
|||||
---|---|---|---|---|---|---|
ADS Desktop | ADS-Lite-E 4 | ADS-Lite-A 5 | ADX | OAS | ||
Total engines | 14 6 | 5 7 | 4 8 | 1,000 9 |
OASMIN: 0 OASSTD: up to 2 |
|
Simultaneous SMP users | 5 | 5 | 5 |
10/25/ 50/100 10 |
5 | |
Dynamic values per graphics | 100 | |||||
Results displayed in a global search | 2,000 | |||||
Languages | 18 | |||||
Objects in entire system | 3 million/ 750k (for ADX Site Director Only) | |||||
Objects in device 11 | Limited by SQL Server storage capacity | |||||
Objects within a single folder | 700 | |||||
Characters in the name of an object | 400 | |||||
Characters in the description of an object | 64 | |||||
Nesting levels for object creation | 7 | |||||
Extensions per object | 10 | |||||
Sets for third-party BACnet states text | 1,000 | |||||
Characters for a third-party BACnet states text | 60 | |||||
Members for a multi-value third-party BACnet states text | 500 | |||||
Non-Simultaneous SMP users | Limited only by memory capacity | |||||
SMP user views | Limited only by memory capacity | |||||
Simultaneous browsers per client computer | 2 (Mix of online, SCT, and Simulation) | |||||
DLLR load extension | Limited only by memory capacity. If you plan to attach a large number of load extensions to a single DLLR object, consider the memory limitation. For load extensions attached to one DLLR object, there is a 64 KB text limit for the list of the Loads fully qualified references. Load Limit = (64 x 1024)/average number of characters per load. 1024 Bytes equals 1 KB. For example, if your DLLR object is configured with Loads that have fully qualified references that average 100 characters (including dots) in length, then you can support approximately 650 loads (64 x 1024/100) for that DLLR. If you reach the memory limit, you may need to combine loads. For example, if a site has multiple physical meters, split the meters across multiple controllers and apply appropriate DLLR loads, if possible. Otherwise, use Interlock or Multiple Command objects to reduce the number of loads added to the DLLR. | |||||
DLLR objects | Limited only by memory capacity. |
Type of Metasys Server |
Computer supported platform |
Site Management Portal (SMP) Users (up to) |
Metasys UI Users (up to) |
|
---|---|---|---|---|
Desktop |
Server |
|||
ADS05U |
Yes |
- |
5 |
5 |
OASSTD |
Yes 12 |
Yes 13 |
5 |
5 |
OASMIN |
Yes12 |
Yes13 |
5 |
5 |
ADX10U |
- |
Yes |
10 |
25 |
ADX25U |
- |
Yes |
25 |
25 |
ADX50U |
- |
Yes |
50 |
50 |
ADX100U 14 |
- |
Yes |
100 |
50 |
Site Director with maximum users |
1 to 14 engines |
1 to 25 engines |
1 to 50 engines |
1 to 100 engines |
1 to 300 engines |
1 to 1,000 engines |
---|---|---|---|---|---|---|
ADS05U |
ADS |
|||||
ADX10U |
Small ADX |
Medium ADX |
Medium/Large ADX |
Large/Extra Large ADX |
Extra Large ADX |
|
ADX25U |
Small ADX |
Medium ADX |
||||
ADX50U |
Medium/Large ADX |
|||||
ADX100U |
||||||
For ADS/ADX computer hardware requirements, refer to the Technical Specifications section of this document:
|