Alarm and trending performance guidelines - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
12.0
Revision date
2024-07-17
Product status
Active
Table 1. Alarm and trending performance guidelines
Description

SNE/

SNC

NCE25/

NAE35/

NAE45

NAE55

NAE85

ADS

ADX

OAS Comments
Average maximum number of alarms/events per hour 100 100 100 100 200 1,000 100 This number applies to alarms/events that originate from devices at Release 5.2 or later.
Maximum number of alarms/events per day 2,400 2,400 2,400 2,400 5,000 48,000 2,400 Within a 24-hour period. This number applies to alarms/events that originate from devices at Release 5.2 or later. Supports one daily burst of 25k alarms/events in one hour.
Maximum number of stored alarms/events 1,000 500 1,000 1,000 Limited by SQL Server storage capacity Limited by SQL Server storage capacity Limited by SQL Server storage capacity N/A
Average maximum number of trend samples per hour 1,500 1,500 1,500 1,500 22,500 100,000 1,500 This number applies to trend samples that originate from devices at Release 5.0 or later. The ADX supports one daily burst of 300k trends in one hour.
Maximum number of trend samples per day 36,000 36,000 36,000 36,000 540,000 2,400,000 36,000 Within a 24-hour period. This number applies to trend samples originating from devices at Release 5.0 or later.
Maximum number of stored trend samples Limited by memory usage Limited by memory usage Limited by memory usage 8,000,000 Limited only by SQL storage capacity Limited only by SQL storage capacity Limited only by SQL storage capacity N/A
Note: Alarms and trends from equipment controllers connected to any of these contribute to the overall totals.