The User Properties tab for a RADIUS user defines general information about the user. The RADIUS server sets and controls the fields that appear as read-only. The Metasys system controls all other fields, which are user modifiable and do not affect the account as maintained by the RADIUS server.
Field |
Description |
Default Value |
Required |
---|---|---|---|
RADIUS User Name |
Displays the login name of the RADIUS user. This is a read-only field. |
New User 1 |
Yes |
RADIUS Description |
Displays a description of the RADIUS user. This is a read-only field. |
— |
No |
Password |
Displays a dimmed field because the password is defined and maintained by the RADIUS server. |
— |
— |
Verify Password |
Displays a dimmed field because the password is defined and maintained by the RADIUS server. |
— |
— |
View Blocked Words List |
Displays a dimmed View Blocked Words List link. |
— |
— |
View Password Policy |
Displays a dimmed link to the rules for password complexity. |
— |
— |
Minimum Password Length |
Displays a dimmed field because the password is defined and maintained by the RADIUS server. |
— |
— |
Maximum Password Length |
Displays a dimmed field because the password is defined and maintained by the RADIUS server. |
— |
— |
Single Access RADIUS User |
Allows the RADIUS user to log in to the account once. After logging in once, the account becomes disabled. |
Cleared |
No |
Temporary RADIUS User |
Allows the RADIUS user to access the system as a temporary user. The user can access the account as long as it has not expired. When expired, the user is logged out of the system. |
Cleared |
No |
Expires On |
Allows the administrator to specify the date on which a temporary user's account expires. The account expires at the end of the specified date (midnight), after which the user can no longer access the system. |
The default value is the current date. |
Yes, if temporary user selected. |
User Must Change Password at Next Logon |
Displays a dimmed field because the password is defined and maintained by the RADIUS server. |
— |
— |
User Cannot Change Password |
Displays a dimmed field because the password is defined and maintained by the RADIUS server. |
— |
— |
RADIUS Account Disabled |
If this option is selected, the RADIUS user account has been disabled by the RADIUS server. |
Cleared |
No |
Account Locked Out |
Displays a dimmed field because this property is controlled by the RADIUS server. If this option is selected, the RADIUS user account has been disabled by the RADIUS server. |
— |
— |
User Can Modify Own Profile |
Allows the users to update their own profile information. The administrator can also change or update the profile information by using the User Profile tab. |
Selected |
No |
User Can View the Item Navigation Tree (Default Tree) |
Designates that a user can view the All Items navigation tree. |
Selected |
No |
User Can Disable Alarm Pop-ups |
Allows the user to disable or enable alarm windows. |
Selected |
No |
Access Type |
Specifies the type of access the user has to the system. |
Standard Access |
Yes |