Roles Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
Language
English

The Roles tab allows administrators to provide access privileges to a group of users without editing each individual profile. Administrators assign a user to one or more roles (Figure 1). The Roles tab is the same for both the Metasys local system user and the Active Directory service user.

Figure 1. Roles Tab

Table 1. Roles Tab Parameters

Field

Description

Default Value

Required

Available Roles

Displays the roles to which the selected user is not assigned.

All available roles, minus the USER role

Assigned Roles

Displays the roles to which the selected user is assigned. All users must be assigned to at least one role.

USER

At least one role

Add

Moves the roles from the Available Roles list box to the Assigned Roles list box.

Remove

Moves the roles from the Assigned Roles list box to the Available Roles list box. Also removes all associated access privileges.