Placing Time-of-Day Restrictions - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1
Security Administrator System Technical Bulletin
- Brand
- Metasys
- Product name
- Metasys System
- Document type
- Technical Bulletin
- Document number
- LIT-1201528
- Version
- 10.1
- Revision date
- 2020-01-21
- Language
- English
Procedure
-
Select the user to configure.
-
On the Edit menu, click
Properties. The User
Properties dialog box appears. See Figure 1.
-
Select the Time Sheet tab. See Figure 1.
-
Select the times when users can access the system by clicking time slots to
toggle between Access Allowed (blue highlight with white
text) and Access Denied (no highlight with black text).
See Table 1.
-
Click OK.