Warning Banners - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
If a Warning Banner is enabled on the Site object, a special warning statement appears every time you launch the SMP UI. To configure this setting, navigate to the Site object of the Site Director and click the Site View tab. In the Warning Banner section, select one of the following:
  • U.S. Department of Defence (DOD) Warning Banner
  • U.S. General Services Administration (GSA) Warning Banner
  • U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA) Warning Banner

The selection may take up to five minutes to become effective.

Once enabled, Warning Banners appear for all local, Active Directory service, and RADIUS users when they log in to the SMP UI. Active Directory and RADIUS users must agree to the conditions on the warning statement before access is granted. Warning Banners do not appear when you log in to SCT.

Figure 1. Warning Banner Selection List on Site Object