To configure a RADIUS account, use the Security Administrator system.
- Using Metasys Launcher, start and log in to the SMP with any Metasys system administrator account.
- On the SMP UI screen, select . The Security Administrator window appears.
- In the Security Administration
menu, click . The Configure RADIUS screen appears.
Figure 1. RADIUS Configure Option
Figure 2. RADIUS Configuration Screen
- Select the Enable RADIUS Authentication check box to enable the fields on the Configure RADIUS screen.
- Fill in the fields of the Configure RADIUS screen using the information in the following table.
- Click Save.Note: At any time, RADIUS may be disabled by clearing the Enable Radius Authentication check box and applying or saving the configuration. While RADIUS is disabled, only local users can authenticate. Login errors display when a user attempts to log in with a RADIUS account.
Table 1. RADIUS Configuration Fields Field
Value
Description
Enable RADIUS Authentication
Checked or unchecked
Check box to configure and enable RADIUS server authentication. The check box defaults to unchecked. If it is not checked, all fields in the RADIUS Configuration screen are not editable.
RADIUS Server
IPv4 address or a DNS name
IPv4 address of the RADIUS server.
RADIUS Server Port
0 - 65535
Port on the RADIUS server to which Metasys directs messages.
RADIUS Client Port
0 - 65535
Port on the Metasys server that is used to send requests to and receive responses from the RADIUS server.
Note: The default port for RADIUS is 1812.Shared Secret
Text string
A secret that is used to verify the validity of messages sent by the RADIUS server to the client. Knowing the Shared Secret does not grant access to a RADIUS server.
NAS Identifier
Text string
A RADIUS attribute that the client uses to identify itself to a RADIUS server.
Authentication Mechanism
MS-CHAPv2
Mechanism used for server authentication.