The Security Administrator system provides three types of access for user accounts: Standard Access, Basic Access, and Tenant Access.
-
Standard Access allows the
Metasys local system user or Active Directory service user to access
all authorized features of the online SMP UI and the SCT; also allows users to
access the Metasys UI. Note: If you have Standard Access and the Advanced Reporting privilege, you can use the Metasys Advanced Reporting System.
- Basic Access allows the Metasys local system user or Active Directory service user to access all authorized features provided in the Basic Access mode of the online SMP UI; also allows users to access the Metasys UI.
- Tenant Access allows the Metasys local system user or Active Directory service user to access all authorized features of the Metasys UI.
Administrators can assign access types for users on the User Properties tab of the Properties of User Operator dialog box. See Figure 1 and User Properties Tab – Metasys Local User.
Access types must meet the following requirements:
- Each user account can have only one type of access to the Metasys system.
- Users requiring Standard Access, Basic Access, and Tenant Access must have a separate user account for each access type with different user names.
- A user who wants both a Metasys local account and an Active Directory service user account must have separate user accounts for each.
- You can use a user account with Standard Access to log in to the online SMP UI, and the SCT. You cannot use a Standard Access user account to log in to the Basic Access mode of the SMP UI.
- You can use a user account with Basic Access to log in to the Basic Access mode of the SMP UI. You cannot use a Basic Access user account to log in to the Standard Access mode of the SMP UI or the SCT.
- When upgrading the Security Database from a version prior to Release 2.0, each user account defaults to the Standard Access type. A standard administrator can change an account to Basic Access or Tenant Access after the upgrade.
- A user with a Metasys local account must select the Metasys Local option on the login screen for the SMP UI or the SCT. A user who is an Active Directory service user must select the appropriate domain name on the login screen.
- Tenant users cannot be Metasys system administrators and cannot have any of the following system-level privileges:
- System Configuration Tool (SCT)
- Advanced Reporting (Metasys Advanced Reporting system)
- Clear Audit History (clear audit log)