For NAE and SNE series network engines, a Security Database
that is backed up from a Metasys server may include a mixture of Metasys local users and roles with Active
Directory service users. The Download To Device function only restores local
users and roles to the device because network engines do not support Active
Directory service authentication and authorization, even if the NxE is a
Site Director. The Download To Device function informs the user if Active
Directory service users exist within the Security Database but are not
restored because the target device does not support Active Directory service
authentication and authorization. The message that appears in the Completed
Actions screen of ActionQ is: OK - Restore to
non-Active Directory Device (616).