Assigning Users to Roles by Using the User Properties Dialog Box - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
Language
English

Procedure

  1. Select the user to configure.
  2. On the Edit menu, click Properties. The User Properties dialog box appears.
    Note: To remove a role, select one or more roles from the Assigned Roles list and click Remove.
  3. Select the Roles tab.
  4. In the Available Roles list, click one or more roles.
  5. Click Add. The selected roles appear in the Assigned Roles list.
    Note: To remove a role, select one or more roles from the Assigned Roles list and click Remove.
  6. Click OK. The system displays a two-headed icon for each permission assigned to the role you selected.