Metasys software installs Windows services. These services include:
- Device Manager (MetasysIII Device Manager)
- ADS/ADX Action Queue (MetasysIII Action Queue)
- Advanced Reporting Cache Refresh (Metasys Report Cache Refresh)
Upon startup, DBCCT checks the status of the Metasys services as shown in Table 1. The tool displays only the tabs and edit fields needed to configure the installed services. You cannot access these fields and tabs until all installed services are stopped. If the tool detects any services running, the editing fields appear as read-only and a message indicates the detected service. We recommend stopping these services before using the DBCCT.
Application Name | Service or Application Pool Name |
---|---|
ADS\ADX\OAS\ODS |
UI app pool Activity Service app pool Metasys Activity Service Event Service app pool Metasys Event Service TimeSeries app pool Metasys TimeSeries Service Scheduler Service app pool Metasys Scheduler Service Authentication Service app pool Health Service app pool Object Service app pool User Service app pool Metasys III Device Manager Service Metasys III Action Queue Service Metasys app pool |
Advanced Reporting System (ARS) |
Metasys Report Cache Refresh |
Metasys UI (Release 8.0 and 8.1) |
UI_AppPools |