Assigning System Access Permissions - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
Language
English

Procedure

  1. Select the user or role.
  2. On the Edit menu, click System Access Permissions. The System Privileges dialog box appears.
  3. Select an available privilege using Table 1.
  4. Click Add.
  5. Click OK.

    The System Access Permissions are assigned to the selected user or role.

    When you are viewing user system privileges, select the Summarized tab to view all system privileges assigned to the user either directly or by a role. You cannot add or remove privileges from this tab, and it does not appear when viewing role system privileges.