Assigning Users to Roles by Using the Role Properties Dialog Box - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
Language
English

Procedure

  1. Select the role to configure.
  2. On the Edit menu, click Properties. The Role Properties dialog box appears.
    Note: You can also double-click a role to display the Role Properties dialog box.
  3. Select the Users tab.
  4. In the Available Users list, click one or more users.
  5. Click Add. The selected users appear in the Assigned Users list.
    Note: To remove a user, select one or more users in the Assigned Users list and click Remove.
  6. Click OK. The system displays a two-headed icon for each permission assigned to the role you selected.