Use the Security Administrator tool to create Metasys local user accounts and grant Metasys system access to Active Directory service users and RADIUS users. The Audit Log of the Site Director allows you to log specific tasks (audits) using the audit trail. The Security System logs the successful and failed login attempts and all administrative tasks.
To access the Security Administrator system, click
in the SMP UI or SCT.Starting at Release 10.1, the Metasys UI User Management feature facilitates the creation and management of users and their roles, category-based permissions, and privileges directly in Metasys UI Online, without the need to install software on client machines. Administrators can create and manage user details for Active Directory, RADIUS, and Metasys local users. This feature is also available in the Metasys Site Management Portal (SMP).