The Users Tab allows administrators to assign users specific roles (Figure 1). The following example shows that Active Directory service for use by the Metasys system is enabled with a defined set of Metasys local system users and Active Directory service users.
Field |
Description |
Default Value |
---|---|---|
Available Users |
Users Not Assigned to the Role |
All Available Users |
Assigned Users |
Users Assigned to the Role |
— |
Add |
Moves the users from the Available Users list box to the Assigned Users list box. Once in the Assigned Users list box, the role access privileges are granted. |
— |
Remove |
Moves the users from the Assigned Users list box to the Available Users list box. Once in the Available Users list box, the role access privileges are removed. Note: You cannot remove the MetasysSysAgent or
BasicSysAgent user from the ADMINISTRATOR role.
|
— |