MetasysSysAgent (Standard Administrator) is a user account with the ADMINISTRATOR role and the Standard Access type assigned. All Standard administrators can access the full Security Administrator system by using the Metasys system online user interface and the SCT. The initial login username is MetasysSysAgent and it is not case sensitive. For the MetasysSysAgent default password, contact your local Johnson Controls® representative.
Standard administrators can change the access type for any account except MetasysSysAgent and BasicSysAgent to Standard Access, Basic Access, or Tenant Access.
All Metasys local system users and Active Directory service users who are Standard Access administrators can administer other Standard Access Metasys local system and Active Directory service users.