Stopping Metasys Services on the ADS - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
At Metasys 10.0 and later, a batch file can be used for stopping starting, and restarting Metasys Server services. The batch file stops the services in the order listed in Table 1. To run the batch file, do the following:
  1. Browse to C:\ProgramData\Johnson Controls\MetasysIII\Diagnostics\Utilities.
  2. Right-click stop.bat and select Run as Administrator. Click Yes in the User Account Control dialog box. A Command Prompt windows appears and displays the status of the services. When the services stop, the Command Prompt window closes.
    Note: You can also use the batch file to restart services on the ADS. For further information, refer to the ADS/ADX Commissioning Guide (LIT-1201645).