The Time Sheet tab allows administrators to place time-of-day restrictions on user login. Users may log in to the system during any of the selected hours. Users are denied access when they try to log in during unselected hours (Figure 1). The Time Sheet tab is the same for both the Metasys local system user and the Active Directory service user. User access for an Active Directory service user is also controlled by an Active Directory service property called Logon Hours. See Authentication Process.
Field |
Description |
Default Value |
Required |
---|---|---|---|
Time of Day |
Allows administrators to select times when users can access the system. |
All hours selected |
Yes |