Setting Password Account Policies - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1
Security Administrator System Technical Bulletin
- Brand
- Metasys
- Product name
- Metasys System
- Document type
- Technical Bulletin
- Document number
- LIT-1201528
- Version
- 10.1
- Revision date
- 2020-01-21
- Language
- English
Procedure
-
Select the user to configure.
-
On the Edit menu, click
Properties. The User
Properties dialog box appears. See Figure 1.
-
Select the Account Policy tab.
-
Select options using Table 1 (Metasys local users) or Table 2 (Active Directory service users).
-
Click OK.