The System Access Privileges have two dialog boxes: one for the role assignment and one for the user assignment. Administrators assign System Privileges directly to a user or role. System Access Privileges apply to the system as a whole, not to individual categories of objects or items. Table 1 describes all the predefined privileges for System Access Permission.
Permissions |
Permission Privileges |
---|---|
Discard All Events |
Gives the user permission to discard all events. Applies to all events a user can manage through the Manage Item Events action set. This action set should be used carefully because it is a system-wide discard. |
Manage Devices & Sites |
Gives the user the following privileges: Reset Device, Archive Device, Set Date, Set Time, Force Archive of Local Repository (audits and trends), Change Audit Enabled Level, and Remove from Site (offline devices and servers). Handles noncategory-based configuration actions. Note: To disable the All Items Organizer for a
user, you must remove the Manage Devices &
Sites privilege from the available privileges for
the user.
|
View Metasys Status 1 |
Gives the user permission to display and use the Audit Viewer. To display the Audit Viewer, the user must have View permission and View Metasys Status permission. Also, the audit data visible in the Audit Viewer depends on the categories for which the user has View privileges. |
Manage Audit History1 |
Gives the user permission to annotate audit entries. |
Clear Audit History1 |
Gives the user permission to clear the audit log. |
Discard Acknowledged Events |
Gives the user permission to discard acknowledged events. Applies to all events a user can manage through the Manage Item Events action set. See the Discard All Events permission description for information on discarding all events. A user who has the Discard Acknowledged Events permission can discard any event that the user has permission to acknowledge, even if it has already been acknowledged. The Discard Acknowledged Events permission provides a one-step shortcut for the two-step process of acknowledging the event and then discarding the event afterward. |
Advanced Reporting1 |
Gives users with Standard Access permission to access the Metasys Advanced Reporting System. In the Advanced Reporting system, users can run reports to view on a web browser. The Advanced Reporting privilege appears in the list of permission privileges only if Metasys Advanced Reporting System is installed. For more information, refer to the Metasys Advanced Reporting System and Energy Essentials Help (LIT-12011312) . |
Schedule Reports1 |
Gives the user permission to create new Scheduled Reports (Query menu), and to run, modify, reschedule, or delete scheduled reports using the Scheduled Reports Viewer. All users, including those without this privilege, may use the Scheduled Reports Viewer to monitor the status of scheduled reports. |
Snooze All Events |
Applies to all events a user can manage by using the Manage Item Events action set. This action set should be used carefully because it is a system-wide snooze. |
System Configuration Tool |
Gives users with Standard Access at releases earlier than 7.0 the following privileges: Access to SCT, Configure and Simulate using the SCT, Passthru mode, and Import Integration. Gives Users with Basic Access permission to use Passthru mode. Basic Access and Tenant Access users do not have access to the SCT. Note:
|