Restrictions - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
Language
English

The Active Directory service on the Metasys system has the following restrictions:

  • The Active Directory service for use by the Metasys system with SSO login-free access and login access is available for the Metasys server and SCT; it is not available when you log in to an NAE, NCE, SNC, or SNE directly.

  • The Change Password menu option is disabled for an Active Directory service user. An Active Directory service user may not change their Active Directory service user account password through the Metasys system SMP UI.

  • Metasys Active Directory service users cannot log in as Metasys local users. They must use their Active Directory service username, password, and domain name to log in.

  • Existing Metasys local users must not use the reserved characters of @ or \ in their usernames. This restriction is necessary to avoid collision with fully qualified Active Directory service usernames.