The intracomputer password, used
for authentication in inter-device communication, has been removed from the following
devices as of Metasys Release 10.0:
- Network engines
- SCT
- Metasys UI
- NAE Update Tool
- LIPNote: The intracomputer password continues to be used for communications between devices prior to Release 10.0.
Starting with Release 10.0, each device has its own unique Device Key, which is generated during the pairing process. The Site Director stores its own individual device secure key and maintains the keys of all child devices. This transition affects the pairing process between network engines and Site Director from this release onwards. For further information, refer to the Pair NxE with Site Director section in Metasys SCT Help (LIT-12011964).