Integrated Authentication - Metasys - LIT-1201528 - General System Information - Metasys System - 10.1

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
10.1
Revision date
2020-01-21
Language
English

The Metasys server services do not use integrated authentication. SCT has two virtual service accounts, IIS APP\MSEA_SCT_APPPOOL and NT SERVICE\MIIISCTAQ, that uses integrated authentication. The access passwords are managed through Windows and the access password can not be changed.