Viewing site alarms - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
The site alarm list shows all the alarms across all the connected devices. To view the site alarm list, click Alarms in the site navigation bar.

Note: When you are viewing the details of a device, the site menu items appear in the lower part of the navigation bar. In the upper part of the navigation bar, you can see the device menu items that can also contain an Alarms menu. If you click the Alarms menu in the device navigation bar, the device alarm list opens.

On the site Alarms page, you can view two alarm lists:

  • To view the active site alarms, click Active Alarms.
  • To view the last 50 alarms from each device on the site, both the active and the inactive alarms, click All Alarms.

To sort the alarm list, click the column headers.

For more information on Verasys alarms refer to Verasys Alarms Summary Technical Bulletin (LIT-12013648).