The Verasys Enterprise section is used to add the Verasys Enterprise site to a collection of sites so that all user facilities are available in a single location. For information about setting up the Verasys Enterprise site, refer to the Verasys Enterprise Configuration and User Guide (LIT-12012995).
On the Verasys Enterprise tab, you can enable the Verasys Enterprise Services and you can get the device ID that you need to add to the enterprise site. Also within this section, you can subscribe to automatic updates to the SBH from the cloud services, and decide at what time you receive the updates.
The Connected Services tab also shows the status of the enterprise connection and the last time it updated.