To configure binary and analog inputs, complete the following steps:
- Navigate to the Commissioning tab and select the Inputs tab.
- On the Generic IOM Inputs screen, configure the following
fields:
- Set the Present field to Present.
- States Text
- Delay Type
- Off Delay
- On Delay
- Alarm priority
- Alarm Text
- Alarm State
- Alarm Delay
- Select the Point Type of the analog input you are using. You can adjust the Value
of the Point Type to any of the following:
- Temperature
- Humidity
- CO2
- Light Sensor
- Refrigerant
- Building Pressure
- Steam Pressure
- Voltage
- Current
Note: Voltage and current are fully configurable input types that are meant to be used
if a different sensor than what is provided in the VAC1002 accessories list is used. The
IOM home page shows the inputs and outputs status and a changeable graphic.