ZEC firmware download - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
You can use the ZEC firmware download feature to upgrade all the zone controllers in a zoning system through the USB upgrade of the Verasys Zone Coordinator (VZC100). This feature means future enhancements to the zone controllers are possible without physically replacing the hardware. The firmware download supports the following zone controller devices:

  • LC-BYP200-0
  • LC-ZEC310-0
  • LC-ZEC410-1
  • LC-ZEC410-2
  • LC-ZEC410-3
  • LC-ZEC510-x
Note: The download process takes between five and seven minutes for each zone.